Trend Settings for WITS Rate of Change Points

You can display the trend, or movement, of the value of a WITS Rate of Change Point in the form of a graph.

The WITS Rate of Change Point is a type of analog point. Therefore, many of the fields in the Trend section of the Rate of Change tab are the same as those for other WITS analog points. However, a Rate of Change point trend is always linear, so there is no Logarithmic field (see Define an Analog Point's Trend Settings).


Disclaimer

Geo SCADA Expert 2021